AXIS#.CS.DEC
Description
This parameter sets the deceleration value for the controlled stop process.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM See Acceleration Units for details. |
Range |
Depends on units. See Acceleration Units for details. |
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.CS.DEC | 0x5002 | 0x2 | UDINT | - | Acceleration | RW | False |
AXIS2.CS.DEC | 0x5102 | 0x2 | UDINT | - | Acceleration | RW | False |